MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Sending Delay after Bus Voltage Recovery

It is possible to set a global sending delay for all telegrams after bus voltage recovery.

Once the bus voltage has been recovered, all send activities of the device are delayed.

Extended settings

Sending delay

 

Sending delay after bus voltage recovery

(0...255, unit = 1 s)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?