MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Maximum Brightness

In some situations, it may not be possible to discern changes to the brightness at maximum brightness values, or the lighting may generally be too bright. In such cases, you can reduce the maximum dimming value.

If lamps can only be dimmed slightly, check whether the maximum dimming value has been set too low (range 76-100%).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?