MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Manual Operation Settings

On the front side of the master, there is a channel button for each channel and a corresponding yellow LED for indicating the channel status (channel status LED).

In addition to the channel buttons, the device also has device selection buttons (M for the master; E1 for Extension 1; E2 for Extension 2). With these buttons, you first select the device (Master/Extension 1/Extension 2) whose status you want to display or which you want to operate. Manual operation is performed after pressing the Manual push-button and then a channel button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?