MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Weather Alarm Function

The weather alarms are activated globally on the Extended settings tab with the parameter Global settings for roller shutter and blind, and the global settings are parameterized there.

Weather Alarm Function

Extended settings

Global settings for roller shutter and blind

 

Weather alarm function

Disabled

 

Enabled

Monitoring time for wind alarm 1

Disabled

   

1 s ... 12 h

 

Monitoring time for wind alarm 2

Disabled

     

1 s ... 12 h

   

Monitoring time for wind alarm 3

Disabled

     

1 s ... 12 h

   

Monitoring time for rain alarm

Disabled

     

1 s ... 12 h

   

Monitoring time for frost alarm

Disabled

     

1 s ... 12 h

   

Priority of weather alarms

Wind alarm->Rain alarm->Frost alarm

Wind alarm->Frost alarm->Rain alarm

Rain alarm->Wind alarm->Frost alarm

Rain alarm->Frost alarm->Wind alarm

Frost alarm->Rain alarm->Wind alarm

Frost alarm->Wind alarm->Rain alarm

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

-Safety and alarm settings

Weather alarm function

React on wind alarm 1

No

Yes

React on wind alarm 2

No

Yes

React on wind alarm 3

No

Yes

   

Use AND logic for wind alarms

No

Yes

   

Reaction on wind alarm(s)

Up

Down

Move to position

   

Reaction on rain alarm

Disabled

Stop

Up

Down

Move to position

   

Reaction on frost alarm

Disabled

Stop

Up

Down

Move to position

   

Height position at weather alarm in %

0 (0-100)

   

Behavior at end of all weather alarms

No reaction

Up

Down

Move to position prior weather alarm

Accept current automatic position

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?