MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Status of Slats (for Blind only)

The current angle of rotation of the blind slats is provided as a value between 0-100%.

The corresponding status object “Feedback for slat” sends the value on the bus if the drive/slat has reached a fixed position after a movement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?