Safety Function Dimming
The global safety function is activated on the Extended settings tab with the parameter Device safety and the global settings are parametrized there ().
The effect of the safety function can be parametrized here for each channel. You can enable the safety function individually for each switching channel.
The safety function is activated if the safety object receives a telegram with the object value that you defined with the parameter Device safety ().
You can define the reaction using the parameter Behavior at start of safety.
If the safety object receives a telegram with the object value opposite of that for activation, the safety function is canceled and the output adopts the state that you defined in the parameterBehavior at end of safety.
The device then waits for a telegram from an external sender within the globally set cycle time. If such a telegram is not received within the monitoring time, the parameter Behavior at exceeding cycle time is used to determine what is to happen.