Locking Manual Mode
You can control the connected drives via the group objects the for manual operating options or via automatic control. There are two options available for the manual operating options:
-
Move manually to height position and slat opening angle (for blind only) via Up/Down/Step/Stop commands
-
Move manually to height position and slat opening angle (for blind only) using absolute position commands
If you want to stop manual operation temporarily, you can enable lock of manual mode for each output channel:
|
Ext. 1/2 Output 1+2 / 3+4 / 5+6 / 7+8 Blind/roller shutter |
Express settings for blind/roller shutter |
||
|
Locking manual mode |
Disabled |
||
|
Enabled |
|||
|
Manual locking |
At object value "1" |
||
|
At object value "0" |
|||
Depending on the setting, manual operation is disabled or enabled when a new telegram value is received:
-
“Manual locking” = “at object value “0”
If “Manual locking” = “0”: manual operation disabled (manual locking active)
If Manual locking = “1”: manual operation enabled (manual locking inactive) -
“Manual locking” = “at object value “1”
If “Manual locking” = “0”: manual operation enabled (manual locking inactive)
If “Manual locking” = “1”: manual operation disabled (manual locking active)