Staircase Lighting Time Function in Combination with On-delay and Off-delay
Combining a staircase lighting time function with an on-delay results in a delayed start of the staircase lighting function.
The result of combining a staircase lighting time function with an off-delay depends on how you have defined the staircase lighting time function:
In the case of the staircase lighting time function with manual switching off (“0” telegram), the off-delay is started if a premature switch-off telegram is received on the “staircase lighting time object”. Once the off-delay time has elapsed, the output is switched off (released).
In the case of the staircase lighting time function without manual switching off, receipt of a switch-off telegram on the “staircase lighting time object” has no effect. The staircase lighting time function continues to the end and then switches the output relay directly to the “released” state. An off-delay cannot be set.
For staircase lighting time functions with manual switching off and warnings activated, the staircase lighting time function is immediately deactivated with a warning when an “Off” telegram is received. The off-delay elapses. No warning is generated.