MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Safety Function Roller Shutter

Safety Function Blind

The global safety function is activated on the Extended settings tab with the parameter Device safety and the global settings are parameterized there.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Safety function

-Safety and alarm settings

Safety function

Disabled

Enabled

 

Behavior at start of safety

No reaction

Stop

Up

Down

Move to position

 

Height position at start of safety in %

0 (0-100)

   

Slat position at start of safety in %

0 (0-100)

   

Behavior at end of safety

No reaction

Up

Down

Move to position prior safety

Accept current automatic position

   

Behavior at exceeding cycle time


No reaction

Stop

Up

Down

Move to position

   

Height position on exceeding cycle time in %

0 (0-100)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?