Group Objects of Automatic Mode of Roller Shutter
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
148 |
Extension Output 1+2 name of the channel |
Movement in automatic mode |
1 bit |
Received |
1.008 Up/DOWN |
|
149 |
Extension Output 1+2 name of the channel |
Stop in automatic mode (roller shutter) |
1 bit |
Received |
1.007 Step |
|
150 |
Extension Output 1+2 name of the channel |
Height position in automatic mode |
1 byte |
Received |
5.001 Percent (0...100%) |