MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Interrupting a Delay Function

If a delay function is started by receiving a new object value and the output channel receives a telegram with the opposite object value during the current delay time, the delay function is canceled. The relay is not switched:

  • Receipt of the object value “0” interrupts an active on-delay.

  • Receipt of the object value “1” interrupts an active off-delay.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?