MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Appropriate ETS Version

The application is compatible with ETS5 and later versions.

Earlier versions, such as ETS3 and ETS4, are not supported.

Application files (knxproj) are optimized for the specific ETS version. If you attempt to load an ETS4 application into ETS5, it will result in unnecessary conversion time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?