MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Name of the Channel

You can assign a separate name for each channel, e.g. "Blind Kitchen". The name of the channel now appears on the parameters, channels and associated group objects.

Ext. 1/2
Output 1+2 / 3+4 / 5+6 / 7+8
-Blind/Roller shutter

Express settings for blind/roller shutter

Name of the channel

Blind Kitchen

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?