MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Number of Additional Steps = 1

Master/Ext. 1/2 Output 1-2: Dimming

User-defined dimming curve

-User-defined dimming curve

Number of additional steps

1

   

A: Minimum brightness in %

22

   

(S1) step 1: KNX value

50

   

(S1) step 1: Brightness value

60

   

B: Maximum brightness in %

100


Dimming curve: User-defined dimming curve with number of additional steps = 1

You will find the parametrized dimming range on the Y-axis.

The minimum brightness (Minimum Brightness) and maximum brightness (Maximum Brightness) can be limited.

The KNX value range (0-100%) is located on the X-axis.

The additional step S1 is defined by the coordinates KNX value (S1) and brightness value (S1). The brightness value should always be greater than the previous value and less than the next value. The dimming curve must always rise and must not fall in certain segments.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?