MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Dimming Range

The technical dimming range is defined by the range between the minimum and maximum brightness of a lamp, and can be set with the aid of a dimmer.

The minimum brightness value that can be set corresponds to a dimming value of 1%, and the maximum brightness value that can be set corresponds to a dimming value of 100%.

The dimming range can be limited further using the software application. This limit can be set individually for each output channel.

Dimming curves can be selected for different lamps.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?