MTN6710-0102S / MTN6810-0102 / MTN6805-0008

User-defined Dimming Curve

A user-defined dimming curve can be stored for special lamps or dimming behavior.

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

Dimming curve

User-defined

 

-User-defined dimming curve

User-defined dimming curve

 
   

Number of additional steps

1 (0-3)

The number of steps (points) in the curve can be set from 0 to 3.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?