MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Using LED and ESL/CFL Lamps

  • Do not use LED lamps in conjunction with energy-saving lamps (ESL/CFL). If possible, use lamps from the same manufacturer and of the same type in order to achieve satisfactory dimming properties.

  • The max. power of each channel is generally lower for LED or energy-saving lamps than for other loads. The maximum loads and derating based on the ambient temperature and devices configuration is defined in the user manual.

  • In Special (RL-LED) mode, the values are significantly reduced once again.

  • The max. power depends heavily on the LEDs and energy-saving lamps used. If the load is too high, the actuator dims to minimum brightness or switches off directly. If this happens, reduce the number of lights.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?