MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Components and Programming Environment

The device is commissioned using KNX-certified software. The application and the technical descriptions are updated regularly and you can find them on the Internet.

This application runs in conjunction with ETS software version 5 or higher.

NOTICE
ETS5 function Partial download shall not be used.
To program the application safely after changes of parameters and group addresses, please use only:
  • Full download [Ctrl + Shift + L]
  • Download Application [Ctrl + Shift + Alt + D]
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?