Switching
You can choose between the switching modes Switching and Blinking. In Switching mode, the relay opens and closes depending on the KNX telegram and the setting for the contact mode.
Ext. 1/2 Output 1-8 -Switch: Switching |
Express settings for switching |
||
Switching mode |
Switching Blinking |
||
Contact mode |
Normally opened Normally closed |
The settings for Output 1 are described below, but apply equally to all outputs.
If you select switching mode Switching for output 1 on the extension, an ETS channel with the name Extension 1 Output 1 - Switch +Name of the channel will be created. All the group objects for this output are located there.