Group Objects for Failure Indicator
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
27 |
Master |
Fault - Internal |
1 bit |
Sending |
1.001 Switch |
|
28 |
Master |
Fault - External |
1 bit |
Sending |
1.001 Switch |
The Fault – Internal object signals internal device faults detected during the self-test. The Schneider-Electric Device Firmware Update Tool can be used to diagnose the fault with the integrated diagnostics function.
The Fault – External object signals external installation faults. The Schneider-Electric Device Firmware Update Tool can be used to diagnose the fault with the integrated diagnostics function.