MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Locking Function

Locking Function

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Locking function

-Automatic, Locking & Calibration settings

Locking function

Disabled

Enabled

 

Lock

At object value "1"

At object value "0"

   

Status of locking signal

Disabled

Enabled

   

Behavior at start of locking

No reaction

Stop

Up

Down

Move to position

   

Height position at start of locking in %

0 (0 – 100)

   

Slat position at start of locking in %

0 (0 – 100)

   

Behavior at end of locking

No reaction

Up

Down

Move to position prior locking

Accept current automatic position

   

Behavior after download

Disabled

Enabled

As before download

   

Behavior after bus voltage recovery

Disabled

Enabled

As before bus voltage failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?