Priority Function (Priority Control)
If you have chosen the priority function (known in other devices as priority control), a new group object called Priority is available for this channel.
The object values of the priority object have the following meaning:
Value bit 1 |
Value bit 2 |
Behavior of output |
---|---|---|
1 |
1 |
Activate priority, switching state "Pressed" |
0 |
1 |
Deactivate priority, switching state dependent on the parameter Behavior at end of priority |
1 |
0 |
Activate priority, switching state "Released" |
0 |
0 |
End of priority, switching state dependent on parameter Behavior at end of priority |
The priority is activated if the value “1” is received on bit 1. The assigned output relay is then switched, depending on bit 2, to “Pressed” (bit 2 = “1”) or “Released” (bit 2 = “0”).
An active priority is deactivated by a new telegram with the value “0” on bit 1. As long as a priority function is active, the channel concerned cannot be controlled by the “switch object” and the advanced functions (central function, time functions, scene function).
After the end of a priority, the behavior of the output relay is determined by the parameter Behavior at end of priority.
The setting Follows currently valid state has the following effect:
During the active priority, all switching commands of subordinate functions are tracked by the application and the switching state is tracked internally. In this way, at the end of the priority, the switching state can be set that would currently have been set without the priority.