MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Manual Switching off

Both staircase lighting time functions enable you to switch off the staircase lighting time prematurely. After receiving the object value 0, the output is switched to the released position.


Manual switching off = Active (“0” telegram)


Manual switching off = Not active (“0” telegram)

A telegram with the object value 0 has no effect. The set staircase light time continues to run normally until the end.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?