MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Failure and Download Behavior

You can enable this function individually for each dimming channel. The behavior of the dimming output in the case of a bus voltage failure / bus voltage recovery and application download is defined.

Master/Ext. 1/2 Output 1/8: Dimming

Failure and download behavior

 
– Safety and alarm settings

Failure and download behavior

Disabled

Enabled

 

Output after bus voltage failure

No reaction

Switch Off

Switch on at selectable brightness

   

Brightness after bus voltage failure in %

100 (1-100)

   

Output on bus voltage recovery

As before bus voltage failure

No reaction

Switch Off

Switch on at selectable brightness

   

Brightness after bus voltage recovery in %

100 (1-100)

   

Output at end of download

As before download

No reaction

Switch Off

Switch on at selectable brightness

   

Brightness after download in %

100 (1-100)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?