MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Connected Nominal Voltage

Extended settings

Global settings for dimming

 

Connected nominal voltage

220-240 V~

110-127 V~

This voltage information is required to ensure optimum zero crossing detection (synchronization with higher/lower voltage level) of the mains voltage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?