MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Blind Type: Downwards Closed/Upwards Horizontal

(Without operating position)

  • Upward movement:
    Slats in horizontal open position (slat position 0%)

  • Downward movement:
    Slats closed downwards (slat position 100%)

  • Possible adjustment range for the opening angle of the slats:
    0-100%


Downwards closed/upwards horizontal


The parameter Slat position after movement in % allows you to define the behavior of the slats after a movement for the channel. If you set the parameter to Operating position, you can set an opening angle to be adopted by the slats after every downward movement.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind

Express settings for blind

 

Slat control

 

Movement of the existing blind

Downwards closed / upwards horizontal

Slat position after movement in %

Last slat position

   

No reaction

   

Operating position

   

Operating position of slat in %

50

The preset value of 50% corresponds to a slat opening angle of about 45°. Since this position is set on a time-controlled basis, please refer also to the section Slat Rotation Time.


NOTE: Unless otherwise indicated in the following instructions, the examples refer to this type of blind.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?