MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Status Response for Switching

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Status response for switching

Disabled

Enabled

The value of the signal object of a channel always corresponds to the current output state (ON or OFF).

Dimmed corresponds to the ON setting. Every time the state changes from OFF to ON or vice versa, the current object value is sent to the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?