MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Reference Movement after Initialization

The reference movement after a download or bus voltage recovery serves to obtain an exact starting position for further positioning movements.


NOTE: The reference movement after initialization is always carried out, even if the function “General reference movement” is disabled.


The reference movement is triggered by an absolute positioning command. These include, for example, receiving a value on the objects “Height position in manual mode” or “Height position in automatic mode”, the calling of scenes, or movement to an absolute position in the case of weather alarm, alarm or lock. If, after initialization, the object “Move object in manual mode” receives a value that moves the blind / roller shutter to the upper end position, the actuator automatically evaluates this movement as a reference movement.


The reference movement after initialization is generally carried out towards the upper end position. If you have enabled sending of the status messages “Feedback for height” and/or “Feedback for slat” , this automatically sends the current status.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?