Number of Scenes
|
Ext. 1/2 Output 1-8 -Switch: Switching |
Scene settings |
||
|
Scenes settings |
Required number of scenes |
1 (1 – 16) |
You can use the scene function to include multiple channels in a scene control. Up to 16 different scenes are available for each output channel.
Each of the 16 scenes can be disabled again.
|
Ext. 1/2 Output 1-8 -Switch: Switching |
Scene settings |
||
|
Scenes settings |
Scene 1 (1-16) |
Disabled Enabled |
|
|
Scene 1 Description |
|||
|
Scene 1 Address (0-63) Dependent: Global Settings for Scenes |
Scene address 0 - 63 |
||
|
Scene 1 Address (1-64) Dependent: Global Settings for Scenes |
Scene address 1 - 64 |
||
|
Scene 1 switching state |
Released Pressed |
For clarity, a short description can be stored for each scene.
Each of these scenes can be assigned one of 64 possible scene addresses 0 to 63 (corresponding to telegram values 0-63) or 1 to 64 (corresponding to telegram values 0-63). This depends on the global settings for scenes.
You can store the switching states (pressed, released) as scene values for each output channel.