MTN6710-0102S / MTN6810-0102 / MTN6805-0008

On-delay and Off-delay

Due to the delay functions, the change of relay states is not carried out immediately after receipt of a telegram, but only after the set delay time has elapsed:

After the object value “1” has been received, the on-delay delays the switching of the relay contact from the released state to the pressed state.

After the object value “0” has been received, the off-delay delays the switching of the relay contact from the pressed state to the released state.

You can also use both functions together with a single channel.


Objects

For each channel, you can parameterize whether the delay affects the switch object, staircase lighting time object or scene object, or multiple objects in combination.


On-delay and off-delay (normally opened/normally closed)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?