MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Extended Settings for Dimming

On the Express settings for dimming tab, activate the Extended settings for dimming.

Master/Ext. 1/2 Output 1 – 2: Dimming

Express settings for dimming

No

Yes

-Dimming times

Dimming times

 

-Time settings

Staircase lighting time

 
   

On-delay time

 
   

Off-delay time

 
 

-Locking & Priority settings

Priority function

 
   

Locking function

 
 

-Safety and alarm settings

Safety function

 
   

Alarm function

 
   

Failure and download behavior

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?