MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Staircase Lighting Time Fix

With Staircase lighting time fix, you can parameterize a fixed staircase lighting time for each channel. The staircase lighting time can be parameterized between 5 seconds and 1 hour. This function makes the Staircase fix object (1 bit) available to you.

Master/Ext. 1/2 Output 1 – 2: Dimming

Staircase lighting time fix

 
– Time settings

Manual switching off

Active

Not active

 

Time extension


Not retriggerable

Retriggerable

Retriggerable and adding

   

Max. number of additions

2 (2 - 5)

   

Duration time

2 min (5 s - 1 h)

   

Switch-Off Prewarning

Disabled

Enabled

     
 

Warning starts (5...255, unit = 1s) before end

30 (before end)

   

Note: Staircase duration time must be longer or equal than prewarning start time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?