MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Scene Names

This parameter is used to define the scene numbering view for the user in the ETS. Either Scene address 1 – 64 or Scene address 0 – 63. The values on the bus are always 0 – 63.

Extended settings

Global settings for scene

 
 

Naming of the scenes (The values on the bus are always 0-63)

Scene address 0 – 63

     

Scene address 1 – 63

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?