MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Behavior of the Output after Bus Voltage Recovery

In the case of bus voltage recovery, the output can adopt a parametrized state.


Possible settings:

  • No reaction
    The output channel remains at its current brightness value.

  • Switch Off
    The output channel is switched off.

  • Switch on at selectable brightness
    The initial brightness is determined by another parameter. The selectable brightness can be set between 1% and 100%.

  • As before bus voltage failure
    With the parameter As before bus voltage failure, the output adopts the state that was saved in the device at the time of the bus voltage failure. Any subsequent manual switchings are overwritten.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?