MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Type of Delay

Delay times can be parameterized for each channel. You can use parameters to define the set delays as Retriggerable or Not retriggerable. In the case of a retriggerable on-delay, the delay time is restarted when a “1” telegram is received. In the case of retriggerable off-delays, the delay time is restarted when a “0” telegram is received.


Retriggerable on-delay (“1” telegram)


Retriggerable off-delay (“0” telegram)

Moreover, for the off-delay, you can also select Retriggerable and adding. The delay time is added when the same telegram value is received, e.g. using a separate button. You can define the maximum number of additions.


Retriggerable off-delay and adding (“0” telegram)

In the case of not retriggerable delays, by contrast, the relay will switch off at exactly the moment the time elapses.


Not retriggerable on-delay


Not retriggerable off-delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?