Number of Additional Steps = 0
Here you receive a linear dimming curve that is limited by the minimum brightness (Minimum Brightness) and maximum brightness (Maximum Brightness).
|
Master/Ext. 1/2 Output 1-2: Dimming |
User-defined dimming curve |
||
|
-User-defined dimming curve |
Number of additional steps |
0 |
|
|
A: Minimum brightness in % |
22 |
||
|
B: Maximum brightness in % |
100 |
||
You will find the parametrized dimming range on the Y-axis.
The minimum brightness (Minimum Brightness) and maximum brightness (Maximum Brightness) can be limited.
The KNX value range (0-100%) is located on the X-axis.