MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Contact Mode Normally Closed

If the switch object receives a telegram with the value “0”, the contact is closed. If a telegram value of “1” is received, the contact is opened. The settings “Pressed” and “Released” are used for the different switching states of the output contacts.

In relay mode Normally closed:

  • Pressed = contact opened

  • Released = contact closed


Switching (Normally closed mode)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?