MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Failure Indicator

The failure indicator of the device can be activated in the ETS. Failure indication is carried out using two group objects.

Extended settings

Device health

 
 

Enable outputs for failure indication

Disabled

     

Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?