MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Priority

The alarm function is a 1-bit group object with high priority. The device safety function has the highest priority. The priority order for switching can be defined globally (Priority of Functions for Switching). The alarm object takes precedence over the following group objects:

  • The priority relative to the locking object / priority object is defined centrally for switching: Priority of Functions for Switching

  • Logical input object

  • Scene object

  • Central switch object

  • Staircase fix / Staircase variable object

  • Switch object

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?