MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Startup Delay

Some motors do not bring full power directly when switched on, but only after a few milliseconds. You can use the time setting for the start-up delay to compensate for this.

A value = 10 gives a start-up delay of 2 x 10 ms = 20 ms

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Extended drive timing

-Extended drive timing

Startup delay (0...255, unit = 10 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?