MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Send Status of Manual Operation via Object

In addition to the possibility of enabling manual operation via the Enable manual operation object, it is also possible to send the status of the manual operation via the Status of manual operation object. You can read the current operating status from the manual operation LED and you will receive feedback via the Status of manual operation object if you have enabled this function.

Extended settings

Manual operation settings

 

Send status of manual operation via object

No

   

Yes

Once Send status of manual operation via object has been enabled, the group object appears.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?