MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Relay Behavior after Bus Voltage Recovery

In the case of bus voltage recovery, the relay can adopt a parameterized state.


Possible settings:

  • Stop: the drive stops immediately.

  • Up: the drive moves to the upper end position.

  • Down: the drive moves to the lower end position.

  • Move to position: the drive moves to the defined position for height and slat (for blind only).

  • As before bus voltage failure: With the parameter “As before bus voltage failure”, the relay adopts the state that was saved in the device at the time of the bus voltage failure. Any subsequent manual switchings are overwritten.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?