PKR39809-02

Appendix J.1 ­ flexVUE Menu Structure

The flexVUE menu structure consists of a main menu and three sub-menus, Alerts, Operator, and Engineer.

The LCD display consists of 2 x 20 character lines. The top line is the page title and the bottom line could be either a sub title or a setting.

When the operator interface is turned on, or if the Menu key is pressed at any time while the operator interface is on, the display will go to the Main Menu with the Alerts Menu as the sub title.

Pressing the Right Arrow when this screen is displayed will navigate to the Alerts menu and display any alert that is active at the time.

Pressing the Down Arrow will display the Operator menu which can then be entered by pressing the Right Arrow.

Pressing the Down Arrow again will display the Engineer menu which can then be entered by pressing the Right Arrow.

ACR

AS

The following table presents the procedure for finding a setting on the
flexVUE O.I.:

Step

Action

1

Press MENU to bring up the menu navigation.

2

Use the Up and Down arrow keys to find the next required menu.

Example: ENGINEER MENU

3

Press SELECT or the RIGHT arrow key to enter the next menu in the navigation structure.

Example: PROTECTION MENU

4

Repeat steps 2 and 3 to continue through the indicated menu navigation.

Example: DIRECTIONAL ELEMENTS > DIRECTIONAL BLOCKING > SEF

5

Scroll through the settings (shown in title case) to the required setting.

Example: Minimum Vzps

6

For information on changing settings, refer to Chapter 4 Operator Functions.

NOTE: On the flexVUE O.I. menu navigation, menus are shown in capitals and editable settings are shown in title case.

Operator Menu

The Operator menu consists of four sub-menus, three of which have their own sub-menus.

ACR

AS

Engineer Menu

The Engineer menu has four sub-menus all of which have further sub-menus. Two more sub-menus can be added.

ACR

AS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.