PKR39809-02

Quick Action Keys (QAK)

Actions that are most likely to be performed by line personnel can be linked to the 12 QAK of the flexVUE interface.

Selecting a quick action will apply that action without any additional confirmation and the lamp next to the key can be used to indicate when the action is active.

A typical action is to toggle features on/off, for example: Work tag ON/OFF LOCAL/RM ; Ground fault protection ON/OFF; etc. The action keys can also be configured to turn options ON, such as protection groups. For example, pressing the Protection Group B key will make Group B active and therefore deactivate whichever group was active prior to the key press.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.