PKR39809-02

Fault Detection Enhancements

There are some detection enhancement features that can fundamentally change the operation of the detection function from the way it has already been described.

All of these enhancements are either off or unavailable by default and will not change the way the detection operates unless evoked by the user.

Each of these functions listed below can be either turned on or made available in WSOS in the Detection group in Feature Selection.

  • Sequence Reset Clears Fault Flags

  • Extended Standard Detection

  • Extended Maximum Time per Curve

  • Per Element Detection

  • Close on Fault Trip

Feature Selection/Detection can be found in WSOS by navigating to:

Display > Configuration > Feature Selection > Detection

With the exception of Per Element Detection and Close on Fault Trip, these features can also be evoked on the O.I..

Sequence Reset Clears Fault Flags

Extended Standard Detection

Extended Maximum Time per Curve

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.