PKR39809-02

Example

If the CLP settings are:

Cold Load Time 180 minutes

Cold Load Multiplier x3

And it is expected that the Setting Currents need to be doubled for the anticipated increase in load.

That can be achieved by setting the Cold Load Operational Time to 90 minutes as shown below.

Changing the Operational Cold Load Time automatically changes the Operational Cold Load Multiplier according to the active Cold Load settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.