PKR39809-02

Display Groups

There are a minimum five display groups in the setVUE menu system and a sixth one for automation if an automation feature is available.

Figure 20
setVUE O.I. Menu structure

The display group a page being displayed belongs to can be identified by the letter that appears in the top right hand corner of the screen.

Table 6 setVUE O.I. Menu Identifiers

Code Display Group

S

System Status

E

Event Log

M

Measurement

P/D

Protection/Detection(1)

A

Automation

C

Communications

(1) Display group P is displayed for an Auto Recloser and will be substituted by a D for an Auto Sectionaliser.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.