PKR39809-02

Launching the IOEX Configuration Tool

The IOEX configuration tool can be launched by selecting

IOEX> Configure ADVC IOEX Mappings in the Customize menu when WSOS is off-line.

That will open the Open OCP Configuration dialogue box shown below.

Figure 40
WSOS File Options page

Choose New or Existing depending on whether a new IOEX mapping file is being created or an existing file is being opened.

Complete the setup information and select OK.

That will leave the IOEX Configuration Tool open to configure a new mapping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.