PKR39809-02

Ground Fault Neutralizer

The Ground Fault Neutralizer (GFN) features allows the PowerLogic ADVC Controller protection to better deal with Earth and Sensitive Earth Faults in systems with resonant earthing along with GFN/Rapid Earth Current limiting devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.