PKR39809-02

Power Measurement

The PowerLogic ADVC Controller can calculate:

  • Real power in kW

  • Reactive power in kVAR

  • Apparent power in kVA

  • PF

On a three phase and per phase basis.

Real and reactive power can be either signed or unsigned as configured in WSOS on the Measurement page:

Power Signed or Unsigned can also be selected on the
operator interface.

NOTE: Signing only applies to Real and Reactive Power. Apparent Power and PF are not signed values.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.